Define Reference Parameter

Reference parameters are similar to derived and predicted parameters. Derived and Predicted parameters receive values from calculation and predictive algorithm respectively, whereas the Reference parameters receive values from the performance curves.

Perform the following steps to define reference parameters:

  1. Select the Reference parameters needed for this system template by selecting the check box next to the parameters.

    You can also search the required parameters using the search box in the top right corner of the window.

  2. Click Add.

  3. Click Save.